您选择的产品已被添加至购物车

Edmund Optics®

资源库

 经由我们 240 多位全球工程师创建且经过验证的可信技术资源库。

滤光片
Search Results for: Cailabs Canunda 反射轴锥镜 (228)

金刚石车削离轴抛物反射镜的粗糙度

Learn about spatial frequency errors and surface roughness of Single Point Diamond Turned off-axis parabolic mirrors at Edmund Optics.

立即查看 添加到收藏夹

反射镜介绍

Mirrors are commonly used to fold or compact an optical system.

立即查看 添加到收藏夹

有柄反射镜

Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.

立即查看 添加到收藏夹

适用于激光应用的高反射率反射镜

The industry standard method for quantifying reflectivity does not tell the whole story

立即查看 添加到收藏夹

半导体超级反射镜

Semiconductor supermirrors offer high reflectivity and outperform many IR mirrors on the market. Learn more about these new supermirrors at Edmund Optics.

立即查看 添加到收藏夹

超快高色散反射镜

Pulse Compression and Dispersion Compensation for Ultrafast Lasers

立即查看 添加到收藏夹

深入了解锥透镜

Axicons can be used in a variety of different fields. Find out more about axicons and how to use them in applications at Edmund Optics.

立即查看 添加到收藏夹

锥透镜介绍

Axicons are conical-shaped optical components used to create a ring-shaped beam.

立即查看 添加到收藏夹

用于色散补偿的高色散超快反射镜

Learn how Highly-Dispersive Mirrors compensate for dispersion and compress pulse duration in ultrafast laser systems, which is critical for maximizing performance.

立即查看 添加到收藏夹

E 系列运动型光学反射镜调整架

E-Series Kinematic Optical Mounts provide high value and essential features for applications including lab use, prototyping, and system integration

立即查看 添加到收藏夹

反射式光学元件适用于激光应用

Beam Conditioning Optics for UV, IR, and Broadband Lasers

立即查看 添加到收藏夹

高反射率镀膜

Highly reflective (HR) coatings are applied to optical components to minimize losses when reflecting lasers and other light sources.

立即查看 添加到收藏夹

同轴照明

Are you designing a system and debating whether or not to use in-line illumination? Read more about the proper time to use in-line and comparisons at Edmund Optics.

立即查看 添加到收藏夹

反射镜金属镀膜

Want to learn more about metallic mirror coatings? Find information about standard and custom metallic mirror coatings that are available at Edmund Optics.

立即查看 添加到收藏夹

大尺寸万向节光学镜架

爱特蒙特光学(Edmund Optics)提供的大尺寸万向节光学镜架可用于将大尺寸精密光学元件(如反射镜)集成到 OEM 和台式系统中。

立即查看 添加到收藏夹

尽量减小超快系统中的热透镜效应

Specialized coatings can minimize thermal lensing in ultrafast laser systems, which are particularly susceptible to detrimental thermal effects.

立即查看 添加到收藏夹

Reflective Laser Beam Shaping

Beam Shaping for High Power and Short Pulse Durations

立即查看 添加到收藏夹

光学棱镜简介

Learn about the different types of optical prisms, their applications, and how to select the right prism for your specific system.

立即查看 添加到收藏夹

了解显微镜和物镜

Learn about the different components used to build a microscope, key concepts, and specifications at Edmund Optics.

立即查看 添加到收藏夹

Axicon Calculator

立即查看 添加到收藏夹

如何校准单片扩束镜

Monolithic Reflective Beam Expanders are ideal for applications requiring broadband or achromatic beam expansion.

立即查看 添加到收藏夹

激光光学实验室: 扩束镜结构及设计

Laser beam expanders consist of transmissive configurations, with Galilean or Keplerian designs, and reflective configurations, which use a series of mirrors, similar to microscope designs.

立即查看 添加到收藏夹

散射

Dispersion is the dependence of the phase velocity or phase delay of light on another parameter, such as wavelength, propagation mode, or polarization.

立即查看 添加到收藏夹

激光光学实验室:背向反射

Back reflections are created when some or part of your beam are reflected back to the source.

立即查看 添加到收藏夹

f/#(镜头光圈/孔径设)

When it comes to your lens, the f/# is one of the most important settings because it controls multiple parameters. Find out what the f/# controls at Edmund Optics.

立即查看 添加到收藏夹

如何制造非球面透镜

Edmund Optics® manufactures thousands of precision aspheric lenses per month in our asphere manufacturing cell that operates 24 hours a day.

立即查看 添加到收藏夹

需要快速获取非球面透镜?

Need an asphere fast? Edmund Optics' off-the-shelf solutions can be modifed in little-to-no time!

立即查看 添加到收藏夹

单一材料 非球面消色差透镜

Single-Material Aspheric Achromats correct chromatic aberrations with a unique geometry, leading to numerous benefits over conventional achromatic lenses.

立即查看 添加到收藏夹

显微镜物镜的未来

Advances in Microscopy Tackle the Challenges of the Future

立即查看 添加到收藏夹

下一代球面透镜

Traditional spherical lenses are evolving due to the increasing demands of applications. Learn about the future of spherical lenses at Edmund Optics.

立即查看 添加到收藏夹
 
销售和技术专家咨询电话
 
或查看各区域电话
一键式
报价工具
只需输入商品编号